Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22775
  • Release Date : 2018/09/03 17:30
  • Print

Maximum number of connectable modules to LCPU when it is not extended

What is the maximum number of modules to be connected without using an extension/branch module?
Category : 

Answer

Up to 10 modules can be connected in the system as a whole except for the power supply module, CPU module, display unit, RS232C adapter, and END cover.
Some modules take up the space of two modules. Refer to the manual of each module.
Product Name
MELSEC-L Series
Series
L Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries