FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > Use of END cover with the branch module and extension module
FAQ
Use of END cover with the branch module and extension module
Are there any restrictions on the END cover when the L series branch module and extension module are used?
- Category :
Answer
Use an END cover applicable to the following.
- The L6EC whose serial number (first six digits) is "*****2" or later
- END cover with ERR terminal (optional item)
- The L6EC whose serial number (first six digits) is "*****2" or later
- END cover with ERR terminal (optional item)
- Product Name
- MELSEC-L Series
- Series
- Other Modules (terminal block, connector, cable etc.)