FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > Continuous logging
FAQ
Continuous logging
Is it possible to log 20 samples of analog data at intervals of 0.5 seconds using the LCPU logging function?
- Category :
Answer
Yes.
As a guide, the processing time is shown below.For the logging condition, refer to figure 1 below.
- For 16 devices: 2 ms
- For 64 devices: 6 ms

As a guide, the processing time is shown below.For the logging condition, refer to figure 1 below.
- For 16 devices: 2 ms
- For 64 devices: 6 ms

- Product Name
- MELSEC-L Series
- Series
- CPU