FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Necessity of terminating resistors in CC-Link communication
FAQ
Necessity of terminating resistors in CC-Link communication
Is it necessary to connect a terminating resistor to a master module when the master module is connected somewhere between the ends of the network?
- Category :
Answer
No, it is unnecessary.
Terminating resistors are only required at both ends of the network.
Terminating resistors are only required at both ends of the network.
- Product Name
- Network Related Products
- Series
- CC-Link
May I have your opinion?
Related FAQ
- Precautions taken when QJ61BT11 is replaced with QJ61BT11N
- Writing comments into a programmable controller
- Whether or not MC protocol frames can be used after A1SJ71UC24 is replaced with QJ71C24N
- Number of remote registers assigned to a remote I/O station
- Difference between AJ65SBTB1-16DT1 and AJ65SBTB1-16DT2