FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Difference between the CC-Link IE Controller Network and a MELSECNET/H network
FAQ
Difference between the CC-Link IE Controller Network and a MELSECNET/H network
What are the differences between the CC-Link IE Controller Network and a MELSECNET/H network?
- Category :
Answer
The CC-Link IE Controller Network is an improved system that has a higher processing speed and a larger data capacity than the MELSECNET/H network system (PLC to PLC network).
For detailed comparisons between the CC-Link IE Controller Network and a MELSECNET/H network, refer to the following manual.
- MELSEC-Q CC-Link IE Controller Network Reference Manual
Appendix 4 Comparison Between CC-Link IE Controller Network and MELSECNET/H
For detailed comparisons between the CC-Link IE Controller Network and a MELSECNET/H network, refer to the following manual.
- MELSEC-Q CC-Link IE Controller Network Reference Manual
Appendix 4 Comparison Between CC-Link IE Controller Network and MELSECNET/H
- Product Name
- Network Related Products
- Series
- CC-Link IE Controller Network