FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Settings required for transient transmission
FAQ
Settings required for transient transmission
There are multiple MELSECNET/H networks and they each have been connected to a relay station.
Are there any parameter settings required for transient transmission to the CPU module with another network No.?
Are there any parameter settings required for transient transmission to the CPU module with another network No.?
- Category :
Answer
The routing parameter settings are required for transient transmission to the CPU module with another network No.
The request source station, relay station, and request destination station each requires the settings.
For more details, refer to the following manual.
- Q Corresponding MELSECNET/H Network System Reference Manual (PLC to PLC network) 7.4.2 Routing function
The request source station, relay station, and request destination station each requires the settings.
For more details, refer to the following manual.
- Q Corresponding MELSECNET/H Network System Reference Manual (PLC to PLC network) 7.4.2 Routing function
- Product Name
- Network Related Products
- Series
- MELSECNET/H