FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > CC-Link master modules' start I/O No. and refresh devices RX/RY
FAQ
CC-Link master modules' start I/O No. and refresh devices RX/RY
Is it possible to set the start I/O No. assigned to the CC-Link master module as refresh targets for RX/RY?
- Category :
Answer
The I/O numbers used for I/O modules and intelligent function modules cannot be used as refresh targets for RX/RY.
Use the I/O numbers greater than those used by I/O modules and intelligent function modules.
Use the I/O numbers greater than those used by I/O modules and intelligent function modules.
- Product Name
- Network Related Products
- Series
- CC-Link
May I have your opinion?
Related FAQ
- Connecting terminating resistors to the sending end and the receiving end in communication of QJ71C24N
- Difference in specifications between "AJ65BT" and "AJ65SBT" in CC-Link remote I/O modules' model names
- Behavior of special relay in offline simulation
- Terminating resistors for RS-485 communication of LJ71C24
- Reception data read request signal of QJ71C24N not turn ON