FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > About network parameters when building MELSECNET/10 with Q02HCPU-A
FAQ
About network parameters when building MELSECNET/10 with Q02HCPU-A
For a NET10 remote I/O network (A1SJ71LP21) with Q02HCPU-A, related manuals explain how to read SB/SW as shown below.
(1) The Type MELSECNET/10 Network System (Remote I/O network) Reference Manual says that SB/SW data is read
by transferring it to Y, D or other types of devices.
(2) The QCPU-A (A Mode) User's Manual says that the special link registers are read by monitoring D9200 and
the following devices.
How do I read the information equivalent to the data in the link registers SB/SW?
(1) The Type MELSECNET/10 Network System (Remote I/O network) Reference Manual says that SB/SW data is read
by transferring it to Y, D or other types of devices.
(2) The QCPU-A (A Mode) User's Manual says that the special link registers are read by monitoring D9200 and
the following devices.
How do I read the information equivalent to the data in the link registers SB/SW?
- Category :
Answer
Q02(H)CPU-A is the AnUCPU equivalent.
When establishing a MELSECNET/10 network, set the refresh parameter with which SB/SW data is transferred to "Y/D" or other types of devices, as explained in the Type MELSECNET/10 Network System (Remote I/O network) Reference Manual.
M9200 and greater/D9200 and greater are a link information area for MELSECNET (II and B)-compatible A1SJ71AP21/AISJ71AT21.
When establishing a MELSECNET/10 network, set the refresh parameter with which SB/SW data is transferred to "Y/D" or other types of devices, as explained in the Type MELSECNET/10 Network System (Remote I/O network) Reference Manual.
M9200 and greater/D9200 and greater are a link information area for MELSECNET (II and B)-compatible A1SJ71AP21/AISJ71AT21.
- Product Name
- Network Related Products
- Series
- MELSECNET/10