FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Overall cable distance and station-to-station distance in CC-Link networks
FAQ
Overall cable distance and station-to-station distance in CC-Link networks
How long are the overall CC-Link cable distance and the CC-Link station-to-station distance in meters?
- Category :
Answer
The overall cable distance and station-to-station distance depend on the version and the transmission speed.
Figure 1 shows the case with Ver.1.10-compatible CC-Link dedicated cables in use.
Figure1
For more details, refer to chapter 3 in the following manual.
- CC-Link System Master/Local Module User's Manual
Figure 1 shows the case with Ver.1.10-compatible CC-Link dedicated cables in use.
Figure1
For more details, refer to chapter 3 in the following manual.
- CC-Link System Master/Local Module User's Manual
- Product Name
- Network Related Products
- Series
- CC-Link
May I have your opinion?
Related FAQ
- Setting required to skip CC-Link slave station numbers
- How to make the expanded cyclic setting for CC-Link local stations
- Limitation on the number of MELSOFT products that can be connected with the QJ71E71
- Unit of the receive data length used by the QJ71C24N series pre-defined protocol support function
- Transient transmission of the CC-Link IE Controller