FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Model name of the connector used for the FCN connector type CC-Link remote I/O module
FAQ
Model name of the connector used for the FCN connector type CC-Link remote I/O module
What is the model name of the connector used for the FCN connector type CC-Link remote I/O module?
- Category :
Answer
FCN connectors (40-pin connector) are shown below.
- A6CON1 (soldering connector)
- A6CON2 (crimp connector)
- A6CON3 (pressure-displacement connector)
- A6CON4 (soldering connector)
- A6CON1 (soldering connector)
- A6CON2 (crimp connector)
- A6CON3 (pressure-displacement connector)
- A6CON4 (soldering connector)
- Product Name
- Network Related Products
- Series
- CC-Link
May I have your opinion?
Related FAQ
- Link data from communication error stations in a CC-Link network
- CD terminal setting of the QJ71C24N
- Data length for fixed buffer data communications by QJ71E71
- Refresh timing of bit data and word data in the same CC-Link station
- Mixing line topologies with star topologies in the CC-Link IE Field Network