FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Terminal blocks for the MELSEC-F series
FAQ
Terminal blocks for the MELSEC-F series
Are the terminal blocks for the MELSEC series removable?
- Category :
Answer
Whether the terminal block is removable or not differs depending on the series. Types of the terminal blocks for the MELSEC-F series main units are as follows.
Note that when replacing a terminal block with another terminal block, they need to be the same model.
・ FX1S/3S series: Not removable
・ FX1N/FX3G series: Removable
・ FX2N/FX3U series: Removable except for 16-pin terminal block
Note that when replacing a terminal block with another terminal block, they need to be the same model.
・ FX1S/3S series: Not removable
・ FX1N/FX3G series: Removable
・ FX2N/FX3U series: Removable except for 16-pin terminal block
- Product Name
- FX1S, FX1N, FX3S, FX3G, FX2N, FX3U
- Product Category
- Main unit
- Series
- MELSEC-F series