FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Setting day of the week when using the TWR instruction (FX3 series)
FAQ
Setting day of the week when using the TWR instruction (FX3 series)
Is day of the week automatically set in the FX3 series when date is written by using the TWR instruction?
- Category :
Answer
Day of week is automatically set.
When data written to the data register for storing day-of-the-week data is within the setting range (K = 0 to 6), the day of the week to be set for a clock is automatically corrected in accordance with the date.
Day of week setting values: 0 (Sunday) to 6 (Saturday)
When data written to the data register for storing day-of-the-week data is within the setting range (K = 0 to 6), the day of the week to be set for a clock is automatically corrected in accordance with the date.
Day of week setting values: 0 (Sunday) to 6 (Saturday)
- Product Name
- FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
- Product Category
- Main unit
- Series
- MELSEC-F series