FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Scan time while operation of a programmable controller CPU is being monitored using GX Works2
FAQ
Scan time while operation of a programmable controller CPU is being monitored using GX Works2
While operation of a programmable controller CPU is being monitored using GX Works2, the scan time displayed differs from the expected scan time.
Answer
Scan time displayed on GX Works2 is the maximum scan time of the monitor target programmable controller CPU.
To check current scan time, monitor the data in D8010.
To check current scan time, monitor the data in D8010.
- Product Name
- FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
- Product Category
- Main unit, Engineering Software, GX Works2, GX Developer
- Series
- MELSEC-F series