FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Data backup failure
FAQ
Data backup failure
Although the latch (backup) area is set, the data is not latched.
Answer
If the OUT instruction using the device number of the latch target device exists in a sequence program, the latched data may be overwritten by execution of the OUT instruction.
Use the SET instruction instead of the OUT instruction for the device numbers that need to be latched.
Use the SET instruction instead of the OUT instruction for the device numbers that need to be latched.
- Product Name
- FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
- Product Category
- Main unit, Engineering Software, GX Works2, GX Developer
- Series
- MELSEC-F series