FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Distinguishing the usage of standard counters and high-speed counters
FAQ
Distinguishing the usage of standard counters and high-speed counters
How can I distinguish the usage of standard counters and high-speed counters?
Answer
Standard counters offer counting up to 10Hz.
For high-speed input signals which exceed 10Hz, use high-speed counters, interruption function, or another processing method which is not affected by the input filter and operation the cycle of a programmable controller.
For high-speed input signals which exceed 10Hz, use high-speed counters, interruption function, or another processing method which is not affected by the input filter and operation the cycle of a programmable controller.
- Product Name
- FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
- Product Category
- Main unit, Engineering Software, GX Works2, GX Developer
- Series
- MELSEC-F series