FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Assignment of input/output numbers (MELSEC-F series)
FAQ
Assignment of input/output numbers (MELSEC-F series)
How are the input/output numbers assigned? (MELSEC-F series)
Answer
Octal numbers are assigned as input/output numbers for the MELSEC-F series.
The octal number system uses the digits from 0 to 7 → from 10 to 17 → from 20 to 27・・・from 70 to 77 → from 100 to 107.
The octal number system uses the digits from 0 to 7 → from 10 to 17 → from 20 to 27・・・from 70 to 77 → from 100 to 107.
- Product Name
- FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
- Product Category
- Main Unit, Engineering Software, GX Works2, GX Developer
- Series
- MELSEC-F Series