FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Adding two channels of the RS-232C port in the FX3G series
FAQ
Adding two channels of the RS-232C port in the FX3G series
I would like to add two channels of the RS-232C port in the FX3G series. How can I add the communication expansion boards and adapters?
- Category :
Answer
Select the 40-point or 60-point type FX3G series main unit. In this case, two FX3G-232-BDs can be connected. When FX3G-CNV-ADP is used, an FX3U-232ADP can be used instead of an FX3G-232-BD.
- Product Name
- MELSEC-F Series
- Product Category
- FX3G
- Series
- Main Unit