FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Overwriting a current value with the high-speed counter comparison instruction
FAQ
Overwriting a current value with the high-speed counter comparison instruction
The output contact is not set by overwriting the current value with the MOV instruction while using the high-speed counter comparison.
- Category :
Answer
The output contact is activated according to the change of the current value register along with the counting input. Therefore, the value changed by executing the MOV instruction is not set before the next count input is received.
- Product Name
- MELSEC-F
- Product Category
- FX1S, FX1N, FX1NC, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
- Series
- Main Unit