FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Extending the extension cable
FAQ
Extending the extension cable
Is it possible to extend the length of the extension cable to over 65 cm?
- Category :
Answer
It is not possible to extend the length of the extension cable to over 65cm. Place the main unit separately by using the parallel link or N:N Network function or configure a distributed system by using CC-Link or CC-Link/LT.
- Product Name
- MELSEC-F Series
- Product Category
- FX1N, FX1NC, FX3G, FX3GC,FX2N, FX2NC, FX3U, FX3UC
- Series
- Option, Accessories