FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Number of files that can be created inside a CF card in the FX3U-CF-ADP
FAQ
Number of files that can be created inside a CF card in the FX3U-CF-ADP
How many files can be created inside a CF card in the FX3U-CF-ADP?
- Category :
-
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Main Unit
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > I/O Extension
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Accessories
Answer
Up to 63 files can be handled simultaneously. In addition, up to 1000 files can be created by creating FIFO function files. * The total capacity of the files must be within the CF (CompactFlashTM) capacity (specified CompactFlashTM card use ratio).
- Product Name
- MELSEC-F Series
- Product Category
- FX3U,FX3UC
- Series
- Main Unit, I/O Extension, Option, Accessories