FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > M8037 (forced STOP signal)
FAQ
M8037 (forced STOP signal)
Is it possible to set a programmable controller from RUN to STOP by turning on M8037 in the program of the FX series while the programmable controller is running?
- Category :
Answer
Yes, it is possible. To set the programmable controller to RUN again, while the programmable controller is stopped, set the built-in RUN/STOP switch as follows: RUN → STOP → RUN.
- Product Name
- MELSEC-F Series
- Product Category
- FX1S,FX1N,FX1NC,FX3G,FX3GC,FX2N,FX2NC,FX3U,FX3UC
- Series
- Main Unit