FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Setting for installing a memory cassette
FAQ
Setting for installing a memory cassette
Are any settings required for installing a memory cassette to the programmable controller?
- Category :
Answer
When the programmable controller is powered on after a memory cassette is installed, the memory cassette is automatically recognized. After the memory cassette is installed, it is separated from the built-in memory of the programmable controller, and peripherals read/write data only from/to the optional memory.
- Product Name
- MELSEC-F Series
- Product Category
- FX1S, FX1N, FX1NC, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
- Series
- Main Unit