FAQ


FAQAbout Products

- FAQ > Industrial Computer > Industrial Computer MELIPC > MI5122-VW > Regarding failure of communication with MI5122-VW via Ethernet
FAQ
Regarding failure of communication with MI5122-VW via Ethernet
Communication failed with MI5122-VW via Ethernet, what shall I check?
- Category :
Answer
Check the IP address of the connected device for a duplicate IP address.
If your computer has multiple network connections, check that there are no devices with the same IP address
for network connections other than those to which the MI5122-VW is connected.
If your computer has multiple network connections, check that there are no devices with the same IP address
for network connections other than those to which the MI5122-VW is connected.
- Product Name
- MELIPC
- Series
- MI5000