Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 25230
  • Release Date : 2019/09/02 16:01
  • Update : 2019/09/02 16:06
  • Print

Regarding connection of MELIPC by CW Workbench

When connecting to MELIPC by CW Workbench "Connect" operation or "Attach" operation,
a timeout might occur during connection.
What should I do in that case?
Category : 

Answer

A timeout might be occurred when connecting to MELIPC by CW Workbench.
Click the [Advanced ...] button on the "VxWorks Connection" setting screen of CW Workbench to extend
the timeout setting.
 
Product Name
MELIPC
Series
MI5000
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?