FAQ
FAQAbout Products
- FAQ > Industrial Computer > Industrial Computer MELIPC > MI5000 > Regarding automatically restart of Windows
FAQ
Regarding automatically restart of Windows
Is it possible to build a system that automatically restarts Windows when Windows does not start (WIN RDY LED flashes)?
- Category :
Answer
It is possible to build a system to restart Windows automatically by VxWorks user program.
The implementation example is described below.
[Windows start monitoring system]
・ Monitor that the status of "WIN RDY LED" changes from "flashing" to "lighting" with the "CCPU_GetLEDStatus" function.
・ If the status of "WIN RDY LED" does not change to "ON" for a certain period,
the "CCPU_WinReset" function forces the Windows part to restart.
The implementation example is described below.
[Windows start monitoring system]
・ Monitor that the status of "WIN RDY LED" changes from "flashing" to "lighting" with the "CCPU_GetLEDStatus" function.
・ If the status of "WIN RDY LED" does not change to "ON" for a certain period,
the "CCPU_WinReset" function forces the Windows part to restart.
- Product Name
- MELIPC
- Series
- MI5000