Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 37704
  • Release Date : 2020/01/29 18:36
  • Print

Accuracy class index of active energy

What is the meaning of and class0.5S ?
Category : 

Answer

Accuracy class index of active energy is a number which gives the limits of the permissible percentage error as defined in the IEC62053-22.
Product Name
Electronic Multi-Measuring Instrument
Series
ME96SS series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?