FAQ


FAQAbout Products

- FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Saving Data Collecting Servers > Pulse magnification setting of EMU4-PX4(Pulse Input Unit)
FAQ
Pulse magnification setting of EMU4-PX4(Pulse Input Unit)
How to set the pulse conversion rate of EMU4-PX4(Pulse Input Unit) and the pulse factor of EcoWebServerIII? Also, how to deal with one-cycle operation(when the value exceeds the data range and returns to 0)?
Answer
Match the setting values with EMU4-PX4 and EcoWebServerIII.
No need to consider one-cycle operation because it is automatically calculated in EcoWebServerIII.
No need to consider one-cycle operation because it is automatically calculated in EcoWebServerIII.
- Product Name
- Energy Saving Data Collecting Servers, Energy Measuring Units
- Series
- EcoWebServerIII, EcoMonitorPlus