FAQ


FAQAbout Products
- FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Measuring Units > How to measure circuits over 600A (EcoMonitorPlus / Light)
FAQ
How to measure circuits over 600A (EcoMonitorPlus / Light)
How to measure circuits over 600A with an Energy Measuring Unit (EcoMonitorPlus / Light)?
Answer
As shown in the figure below, a current transformer (CT) with a secondary current of 5A is attached to the measurement location, and a split-type current sensor for the Energy Measuring Unit (model name: EMU-CT5-A, EMU2-CT5, EMU2-CT5-4W) is installed on the secondary side of the CT.


- Product Name
- Energy Measuring Units
- Series
- EcoMonitorPlus, EcoMonitorLight