FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding the Connected/Disconnected Module Detection button on FX5-CCLGN-MS
FAQ
Regarding the Connected/Disconnected Module Detection button on FX5-CCLGN-MS
Even if you click the Connected/Disconnected Module Detection button displayed on the "CC-Link IE TSN Network Configuration" setting screen, an error occurs and detection is not possible. Is there a solution?
Answer
For the Connected/Disconnected Module Detection of FX5-CCLGN-MS, the network configuration of the subsequent stages can not be automatically detected unless the network has been established between the FX5-CCLGN-MS operating as the master station with at least one local or remote station.
Use the above function after establishing communication between FX5-CCLGN-MS with one or more local or remote stations.
Use the above function after establishing communication between FX5-CCLGN-MS with one or more local or remote stations.
- Product Name
- FX5-CCLGN-MS
- Product Category
- Network/Communication
- Series
- MELSEC iQ-F Series