FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding the change of settings for reserved station (master station) of FX5-CCLGN-MS
FAQ
Regarding the change of settings for reserved station (master station) of FX5-CCLGN-MS
Is it possible to change FX5-CCLGN-MS to a reserved station by program?
Answer
FX5-CCLGN-MS allows the master station to change the reserved station setting with parameters, but the setting can not be changed by program.
Note that link special registers SW0020 to SW0FFF are areas where the system stores data and can not be changed by the customer.
Note that link special registers SW0020 to SW0FFF are areas where the system stores data and can not be changed by the customer.
- Product Name
- FX5-CCLGN-MS
- Product Category
- Network/Communication
- Series
- MELSEC iQ-F Series