FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding the switching Hubs that can be used for CC-Link IE TSN
FAQ
Regarding the switching Hubs that can be used for CC-Link IE TSN
Which switching HUBs can be used with CC-Link IE TSN?
Answer
The CC-Link IE TSN has a CC-Link IE TSN Class B/A, and the available switching HUBs are also specified by supported standards, synchronization accuracy, etc.
Check the CC-Link Association website for the model name and usage of the corresponding switching HUB.
Check the CC-Link Association website for the model name and usage of the corresponding switching HUB.
- Product Name
- FX5-CCLGN-MS
- Product Category
- Network/Communication
- Series
- MELSEC iQ-F Series