FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding EtherNet/IP Communications
FAQ
Regarding EtherNet/IP Communications
Is EtherNet/IP communication possible on the built-in Ethernet port of the FX5 CPU module?
Answer
The built-in Ethernet port on the FX5 CPU module does not support EtherNet/IP communication.
Use FX5-ENET/IP.
Use FX5-ENET/IP.
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module, Network/Communication
- Series
- MELSEC iQ-F Series