FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding simultaneous access to Web Server function
FAQ
Regarding simultaneous access to Web Server function
What is the maximum number of logins that can be logged in if the same username/password simultaneously accesses the web server function?
Answer
The Web server function allows you to log in from up to four devices at the same time. You can't log in from the fifth machine.
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module, Network/Communication
- Series
- MELSEC iQ-F Series