FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding Simple CPU communication function connection between CC-Link IE Field Network Basic masters within 1 network
FAQ
Regarding Simple CPU communication function connection between CC-Link IE Field Network Basic masters within 1 network
Is it possible to perform data-link between FX5 CPU modules using CC-Link IE Field Network Basic within a single network using the Simple CPU communication function?
Answer
It cannot. Because there will be two CC-link IE field network Basic master stations in a network.
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module, Network/Communication
- Series
- MELSEC iQ-F Series