FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding the number of FX5-4A-ADP connections
FAQ
Regarding the number of FX5-4A-ADP connections
How many FX5-4A-ADPs can be connected to an FX5 CPU module?
Answer
Up to 4 FX5-4A-ADPs can be connected to an FX5U/FX5UC/FX5S CPU module.
To connect 3 or more FX5-4A-ADPs, the FX5-4A-ADP must have a serial number S/N: 224 **** or later.
To connect 3 or more FX5-4A-ADPs, the FX5-4A-ADP must have a serial number S/N: 224 **** or later.
Up to 2 FX5-4A-ADPs can be connected to the FX5UJ CPU module.
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module, Analog
- Series
- MELSEC iQ-F Series