FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding changing the current address (user unit, pulse unit)
FAQ
Regarding changing the current address (user unit, pulse unit)
Is it possible to change the current address (per user, per pulseuser unit, pulse unit) of the built-in positioning function?
Answer
It can be changed.
It is now possible to write to the address (user unit, pulse unit) by the DHCMOV command. However, writing is disabled during positioning operations.
It is now possible to write to the address (user unit, pulse unit) by the DHCMOV command. However, writing is disabled during positioning operations.
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module, Motion/Positioning
- Series
- MELSEC iQ-F Series