FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding EN and ENO
FAQ
Regarding EN and ENO
What are EN and ENO used in functions?
Answer
EN (enable input) ・・・ This is the execution condition of the function.
The function with EN is executed only if the execution condition of EN is TURE.
ENO (enable output) ・・・ Outputs the execution results of the function.
The function with EN is executed only if the execution condition of EN is TURE.
ENO (enable output) ・・・ Outputs the execution results of the function.
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module, Engineering Software
- Series
- MELSEC iQ-F Series