FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding sending emails
FAQ
Regarding sending emails
Is it possible to send emails with the iQ-F series?
Answer
Using the email function of FX5-ENET, it is possible to send mail via a mail server.
The email function is supported in the following versions.
・Hardware serial number: 234 **** or later
・Firmware version 1.200 or later
The email function is supported in the following versions.
・Hardware serial number: 234 **** or later
・Firmware version 1.200 or later
- Product Name
- FX5-ENET
- Product Category
- Network/Communication
- Series
- MELSEC iQ-F Series