FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding the MQTT Communication Function Publish Program
FAQ
Regarding the MQTT Communication Function Publish Program
When publishing with MQTT communication function, can it be programmed only with ladder program without using module FB?
Answer
You can't program it with the ladder program alone. To use the MQTT communication and email functions, you must use the module FB and program it.
- Product Name
- FX5-ENET
- Product Category
- Network/Communication
- Series
- MELSEC iQ-F Series