FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding the QoS function of the MQTT Communication function
FAQ
Regarding the QoS function of the MQTT Communication function
What are the different levels of QoS function?
Answer
There are three QoS levels and FX5-ENET is also supported.
・QoS0 - The message is sent only once from the source client.
Messages are not guaranteed to arrive at the destination.
・QoS1 - The message is retransmitted until it reaches the destination client.
Duplicate messages may arrive at the destination.
・QoS2 - Messages are delivered so that they reach the destination client only once.
・QoS0 - The message is sent only once from the source client.
Messages are not guaranteed to arrive at the destination.
・QoS1 - The message is retransmitted until it reaches the destination client.
Duplicate messages may arrive at the destination.
・QoS2 - Messages are delivered so that they reach the destination client only once.
*The higher the QoS level, the more accurate the message and the higher the quality, but the higher the number of communications, the higher the communication load.
- Product Name
- FX5-ENET
- Product Category
- Network/Communication
- Series
- MELSEC iQ-F Series