FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding multiple connections for the MQTT communication function
FAQ
Regarding multiple connections for the MQTT communication function
Can I open a connection with multiple brokers at the same time with the MQTT communication function of FX5-ENET?
Answer
The MQTT communication function of FX5-ENET does not allow multiple connections to be opened at the same time. The MQTT communication function has a maximum of one connection only.
- Product Name
- FX5-ENET
- Product Category
- Network/Communication
- Series
- MELSEC iQ-F Series