FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding settings when the battery is installed
FAQ
Regarding settings when the battery is installed
Optionally, what are the GX Works3 settings when the battery FX3U-32BL is installed?
Answer
From the GX Works3 settings when the optional battery is installed, it must be set to Installed in the Optional Battery Settings.
Use the following procedure to display the Optional Battery Settings.
Use the following procedure to display the Optional Battery Settings.
From the GX Works3 navigation pane, click Parameters > Module Name > CPU Parameters > Memory/Device Settings > Device/Label Memory Area Settings > Device/Label Memory Area Capacity Setting > Device/Label Memory Area Setting > Detailed settings.
- Product Name
- FX5U,FX5UC,FX5UJ,FX5S
- Product Category
- CPU Module, Engineering Software
- Series
- MELSEC iQ-F Series