FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regrading using the Positioning Function with a Relay-Output Type FX5 CPU Module
FAQ
Regrading using the Positioning Function with a Relay-Output Type FX5 CPU Module
Can the positioning function be used by High-speed pulse I/O module : FX5-16 ET/ES-H to the relay output type FX5 CPU Module?
Answer
High-speed pulse I/O module : The FX5-16 ET/ES-H can be added regardless of the output type of the CPU Module, and the positioning function can be used with the relay output type FX5 CPU Module.
*FX5S CPU Modules are excluded.
*FX5S CPU Modules are excluded.
- Product Name
- FX5U,FX5UC,FX5UJ,FX5S
- Product Category
- CPU Module, Engineering Software
- Series
- MELSEC iQ-F Series