Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 44473
  • Release Date : 2024/07/02 19:06
  • Print

Regarding compatible version of CANopen communication function for PDO communication

When using PDO communication of CANopen communication function with FX5-CCLGN-MS, are there any restrictions on firmware version, etc.?
Category : 

Answer

It is necessary to use the following CPU module, FX5-CCLGN-MS, GX Works3 versions.
 
FX5-CCLGN-MS・・・1.020 or later
FX5U/FX5UC CPU module ・・・1.260 or later
FX5UJ CPU module ・・・1.070 or later
GX Works3・・・1.105 K or later
 
*If the firmware of the FX5-CCLGN-MS does not support the CANopen communication function, a network error (error code: 2221 H) or initialization failure (event code: 00C54) occurs and the data link will not work.
Product Name
FX5-CCLGN-MS
Product Category
Network/Communication
Series
MELSEC iQ-F Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries