Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 44474
  • Release Date : 2024/07/02 19:07
  • Print

Regarding CC-Link IE TSN CANopen Communication function

Which CANopen communication profile does the FX5-CCLGN-MS support?
Category : 

Answer

The CANopen communication functions supported by the FX5-CCLGN-MS conform to the CiA402 CANopen profile, and can control devices that support the CiA402 device profile.
Among the CiA402 control modes, the FX5-CCLGN-MS supports profile position mode (pp), profile speed mode (pv), profile torque mode (pt), and homing mode (hm).
 
See the manual below.
MELSEC iQ-F FX5 CC-Link IE TSN Master/Local Module User's Manual
Product Name
FX5-CCLGN-MS
Product Category
Network/Communication
Series
MELSEC iQ-F Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries