FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding number of servo amplifiers that can be connected via PDO communication
FAQ
Regarding number of servo amplifiers that can be connected via PDO communication
How many servo amplifiers can be connected by PDO communication of FX5-CCLGN-MS?
Answer
The maximum number of servo amplifiers connected to the FX5-CCLGN-MS varies according to the number of axes.
Example: When connecting a 3-axis servo amplifier, the FX5-CCLGN-MS can connect up to 20 stations when the maximum number of connected stations is 60/the number of axes is 3.
Example: When connecting a 3-axis servo amplifier, the FX5-CCLGN-MS can connect up to 20 stations when the maximum number of connected stations is 60/the number of axes is 3.
- Product Name
- FX5-CCLGN-MS
- Product Category
- Network/Communication
- Series
- MELSEC iQ-F Series