Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 20761
  • Release Date : 2018/08/21 16:10
  • Update : 2018/09/05 15:50
  • Print

Regarding the length of the key to be inserted in the hollow shaft of right angle shaft type.

What dimensions are necessary for the key to be inserted into the hollow shaft?
Category : 

Answer

The key size to be inserted into the hollow geared motor should be nearly twice the length of the hollow shaft hole diameter.

In the case of the GM-SSY with service factor 1.0, select the key to double length among 1.5 of the diameter of the hollow shaft.
For the GM-SHY with service factor 1.4, select the key to length from twice to 2.5 times of the diameter of the shaft.
Insert the key so that it fits the end face side of the hollow shaft (H8 tolerance).
Product Name
Geared Motors
Series
Geared Motors Right angle shaft type, S-PM Geared Motors Right angle shaft type
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?