Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 20773
  • Release Date : 2018/08/21 16:10
  • Update : 2018/09/07 14:35
  • Print

Regarding the brake wiring for when the inverter drive is in use.

Answer

When the geared motor is being operated by inverter drive, please do not make connections to the secondary side of the inverter. As for the brake wiring, please use either Separated braking method or Direct current braking method through commercial power. The brake goes into operation late due to low voltage when it starts to operate, and elements within the power unit will be damaged due to PWM waves.
Product Name
Geared Motors
Series
Geared Motors Parallel shaft type, Geared Motors Right angle shaft type, S-PM Geared Motors Parallel shaft type, S-PM Geared Motors Right angle shaft type
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?