FAQ


FAQAbout Products

- FAQ > Drive Products > Geared Motors > Geared Motors Parallel shaft type > Difference between actual gear ratio and nominal gear ratio
FAQ
Difference between actual gear ratio and nominal gear ratio
Please explain the difference between the actual gear ratio and the nominal gear ratio.
- Category :
-
- FAQ > Drive Products > Geared Motors > Geared Motors Parallel shaft type
- FAQ > Drive Products > Geared Motors > Geared Motors Right angle shaft type
- FAQ > Drive Products > Geared Motors > S-PM Geared Motors Parallel shaft type
- FAQ > Drive Products > Geared Motors > S-PM Geared Motors Right angle shaft type
Answer
There are two types of gear ratios for Mitsubishi Geared Motors: nominal gear ratio and actual gear ratio. Nominal gear ratios are represented using integers such as 1/5, 1/10, 1/15, and so forth, and are unified among each model. Actual gear ratios are figures unique to each model.
For example, the GM-S 0.4kW model has nominal gear ratio of 1/30 and actual gear ratio of 1/28.51. (Some makers have the same nominal gear ratio and actual gear ratio.)
For example, the GM-S 0.4kW model has nominal gear ratio of 1/30 and actual gear ratio of 1/28.51. (Some makers have the same nominal gear ratio and actual gear ratio.)
- Product Name
- Geared Motors
- Series
- Geared Motors Parallel shaft type, Geared Motors Right angle shaft type, S-PM Geared Motors Parallel shaft type, S-PM Geared Motors Right angle shaft type