FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Switching between External operation mode and PU operation mode
FAQ
Switching between External operation mode and PU operation mode
I want to switch the External operation mode and PU operation mode with the switch.
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
Assign X16 signal, and set Pr.79 to "0", to switch the operation mode with turning ON/OFF X16 signal.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700